Technical FAQs

Ask a Question

Replacement overload relay for 8536SB contactor

Issue:

What is the replacement melting alloy overload relay for a 8536SB starter

Product Line:

8536SB type starters

Environment:

US Product

Cause:

It is sometimes necessary to replace this overload relay

Resolution:

For a 2 pole unit, use 9065SDO4.  This will require one thermal unit to be ordered separately

For a 3-5 pole unit, use 9065 SDO5.  The thermal units will also need to be ordered separately.
 

Was this helpful?
What can we do to improve the information ?