Technical FAQs

Ask a Question

Does Square D offer separate enclosures for the PowerPact T and U frame circuit breakers?

ISSUE:
Product availability

PRODUCT LINE:
Circuit Breaker Enclosures

ENVIRONMENT:
PowerPact T and U frame Breakers

CAUSE:
Application

RESOLUTION:
No, Square D does NOT offer separate enclosures for the PowerPact T and U frame breakers. However, Square D does published the minimum required dimensions for enclosures:
The T-frame would require an enclosure approximately 40.5" H x 13.78" W x 4.33" D
The U-frame would require an enclosure approximately 40.5" H x 13.75" W x 4.33" D


 
Was this helpful?
What can we do to improve the information ?