Technical FAQs

Ask a Question

What are the dimensions of the non-reversing U-Line starters?

Issue:
What are the dimensions of the non-reversing U-Line starters LUB12, LUB32, LUS12, LUS32?

Product Line:
TeSys U-Line Starters

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
Please see attached PDF for dimensions.
Was this helpful?
What can we do to improve the information ?