Technical FAQs

Ask a Question

What is the generator interlock kit for the HOM1224L125PGC Series S02 load center?

Product Accessories

Product Line:
Homeline load centers

Generator interlock kit.


The HOM1224L125PGC is a Main Lug load center, so to use a generator interlock kit, the load center MUST first be converted to a main breaker load center using the QOM1 main breaker frame size. The QOM1 can be obtained from 50amp up to 125amp maximum for this load center. SEE current digest for Main Breaker catalog numbers.

Once the load center is converted to a Main Breaker, the generator interlock kit catalog number 
HOMCRBGK1 can be used.
Was this helpful?
What can we do to improve the information ?