Technical FAQs

Ask a Question

Are the S-Flex ATV212 enclosed drives CSA approved?

Customer is requesting that the S-Flex drive come with a CSA approval

Product line:
S-Flex, SFD

All models

For use in the Canadian Market

The S-flex is not sold in Canada, however the product is manufactured to cUL (CSA and UL standards).  The standard product only comes with a UL label only.  To get the product with the cUL label, you must build the drive in the Product Selector Tool and in the Notes To Engineering ask for the cUL label.

Was this helpful?
What can we do to improve the information ?