Technical FAQs

Ask a Question

Are the standard selector switch knob and the Gloved-Hand selector switch knobs for K and SK selector switches provided with the supportive secondary ring nut?

Issue:
Are the standard selector switch knob and the Gloved-Hand selector switch knobs for K and SK selector switches provided with the supportive secondary ring nut?

Product Line:
Type K, SK 30mm Push button

Environment:
9001K, 9001SK

Cause:
Assembly/wiring

Resolution:
When purchasing just the selector switch knob, the secondary ring nut that holds the knob to the selector switch or potentiometer must be purchased as a separate item.  Part number is 9001SK46.
Was this helpful?
What can we do to improve the information ?