Technical FAQs

Ask a Question

Are there any current product lines available that can be used to interchange components form the XVAC74B120 tower light?

Issue:
Are there any current product lines available that can be used  to interchange components form the  XVAC74B120 tower light?

Product Line:
XVAC components, XVE Components-70mm diameter

Environment:
XVE, XVA

Cause:
Assembly/wiring

Resolution:
Customers may consider using individual lens units from the XVE line of tower lights and beacons. Be aware that the base of the XVAC is flat and allows it to be mounted directly to a flat surface. The bases of the XVE devices are rounded and require a support tube for mounting. The jewelling on the lens units are slightly different but are functionally the same.
Was this helpful?
What can we do to improve the information ?