Technical FAQs

Ask a Question

What is the Hand-Off-Auto selector switch for an 8536SEA starter in a NEMA 3R enclosure?

Issue:
What is the Hand-Off-Auto selector switch for an 8536SEA starter in a NEMA 3R enclosure?

Product Line:
8536 Type S NEMA Starters

Environment:
US Product Lines

Cause:
The 176 Digest is unclear

Resolution:
The Hand-Off-Auto selector switch you will need is a 9999SC8 which comes as a kit with the selector switch, contact block, HOA nameplate, optional wiring harness and diagram.
Was this helpful?
What can we do to improve the information ?