Technical FAQs

Ask a Question

What is the part number for a coil suppressor for LC1F185G7?

Issue:
What is the part number for the coil suppressor module for LC1F185G7?

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
The 176 Digest does not specify

Resolution:
There are 2 possibilities for coil suppression of a 120V coil:

The LA4FRCF is the part number for 50-110V coil suppressor.

The LA4FRCP is the part number for 127-240V coil suppressor.
Was this helpful?
What can we do to improve the information ?