Technical FAQs

Ask a Question

What is the part number which links the switch mechanism to the float on a 9037HG pressure switch?

Issue:
What is the part number which links the switch mechanism to the float on a 9037HG pressure switch?

Product Line:
9037HG float switches: 9037HG30, 9037HG31, 9037HG32, 9037HG33, 9037HG3, 9037HG34, 9037HG35, 9037HG36, 9037HG37, 9037HG38, 9037HG39

Environment:
US Product

Cause:
The vertical shaft which links the float and switch mechanism on a 9037HG float switch is not defined on the instruction bulletin.

Resolution:
2810G3
Was this helpful?
What can we do to improve the information ?