Technical FAQs

Ask a Question

What does an Error Code 0.30 and faulty ground connection mean on an IG6 ?

 Issue:
Troubleshooting a LIM

Product Line:
Medical Panels

Environment:
IG6,IG6M

Cause:
Error Codes

Resolution:
 
Check to make sure the connector plate ground terminals are connected to the back plate
 
Was this helpful?
What can we do to improve the information ?