Technical FAQs

Ask a Question

Will the QO3100BNF, QO3100BNS or QO3100BNRB accept bolt on QOB circuit breakers?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Application

Cause:
Clarification

Resolution:
These QO circuit breaker enclosures accept only plug on type QO, 3 pole, 100A maximum circuit breakers. They will not accept bolt on QOB circuit breakers.
Was this helpful?
What can we do to improve the information ?