Technical FAQs

Ask a Question

Are auxiliary contacts available for the 4-pole 8903 Type L lighting Contactors?

Issue:
Are auxiliary contacts available for the 4-pole 8903 Type L lighting Contactors?

Product Line:
8903LG40, 8903LF40, 8903LH40, 8903LWW40, 8903LW40, 8903LA40, 8903LO40
8903LXG40, 8903LXF40, 8903LXWW40, 8904LXW40, 8903LXA40, 8903LXO40

Environment:
US product

Cause:
There is no auxiliary contact listing for 4 pole devices in the Digest.

Resolution:
These contactors do not have auxiliary contacts per se.  Adder poles can be added and used as auxiliary contacts in the same way that 6-8 pole versions do.  To accomplish this with the 4 pole versions of this contactor, an additional mounting plate must be installed on the contactor as well. 

For a left side adder deck single pole, order 8903L1L, and for a double pole order 8903L3L.  With either one of these units also order mounting bracket 31071-038-02 and quantity two of screw 21911-12100 (this is a 6-32 X 5/16 screw)

For a right side adder deck single pole, order 8903L1R, and for a double pole order 8903L3R.  With either one of these units also order mounting bracket 31071-038-01 and quantity two of screw 21911-12100 (this is a 6-32 X 5/16 screw)

 
Was this helpful?
What can we do to improve the information ?