Technical FAQs

Ask a Question

What parts do I need in order to replace the disconnect assembly for an 8538, series K, combination starter?

Issue:
What parts do I need in order to replace the disconnect assembly for an 8538, series K, combination starter?

Product Line:
8538 Type Combination Starters

Environment:
US Product Lines

Cause:
There are multiple parts in the disconnect assembly

Resolution:
To order the complete disconnect assembly, you will need to order 9422FTCN30.

If you need to order pieces of the disconnect assembly, see attached PDF for a list of the parts breakdown.
Was this helpful?
What can we do to improve the information ?