Technical FAQs

Ask a Question

9001B Three Button Control Station in NEMA 3R

Is there a NEMA 3R version of the 9001B Control Stations with 3 buttons

Product Line:
9001B Control Stations

US Product

There are NEMA 3R versions of the one and two button stations listed, but of the three button stations

There is no NEMA 3R three button 9001B control station.  The 9001KY/9001SKY may be a suitable alternative.
Was this helpful?
What can we do to improve the information ?