Technical FAQs

Ask a Question

9001BG202 Contact Arrangement

Issue:
What is the contact arrangement for a 9001BG202 control station?

Product Line:
30mm control stations

Environment:
US product

Cause:
The arrangement of the contacts are unclear

Resolution:
The start button is configured with a normally open contact.  The stop button is also configured with a normally open contact.  Both of these contacts are double break.
Was this helpful?
What can we do to improve the information ?