Technical FAQs

Ask a Question

What is the part number for a replacement external reset button for an 8940WE3S2 pump panel?

Issue:
What is the part number for a replacement external reset button for an 8940WE3S2 pump panel?

Product Line:
8940 Class Pump Panel

Environment:
US Product Lines

Cause:
The 176 Digest does not list a replacement

Resolution:
There are 3 numbers to order:

300190-124-65   (Reset Button)
30019-121-01     (Ring Nut)
29206-30700      (Gasket)
Was this helpful?
What can we do to improve the information ?