Technical FAQs

Ask a Question

Is there a thermal sensor part number for the ATV61HD18M3X?

Issue:
Is there a thermal sensor part number for the ATV61HD18M3X?

Product Line:
ATV61

Environment:
All serial numbers for ATV61

Cause:
N/A

Resolution:
ATV61HD18M3X  Is a frame size 6 
The drive thermal sensor part numbers is not listed for frame sizes below frame size 9 , because they is not available for purchase as a seperate spare parts.  
 
Was this helpful?
What can we do to improve the information ?