Technical FAQs

Ask a Question

On the LU2B reversing starters why do we need a coil voltage for the power base?

Issue:    
LU2B32FU vs LUB32: Why do we need to confirm the coil voltage on the reversing power base but not the non reversing one?

Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause: A voltage code is needed in order to order a reversing U line starter, but not the non reversing u line starters.
 
Resolution: The reversing module has a coil that has to match with the control module voltage, the base has a coil which receives the correct voltage it needs from the circuit inside the control module itself (no matter what the input voltage is)


Keywords: U line, LUB, LU2B, tesys U, reversing, voltage code, control voltage
 
 
Was this helpful?
What can we do to improve the information ?