Technical FAQs

Ask a Question

Do we need to order thermal units when using the 9065 type SF and type ST solid state overload relays?

Issue: Do we need to order thermal units when using the 9065 type SF and type ST solid state overload relays?


Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause: Do we need to order thermal units when using the 9065 type SF and type ST solid state overload relays?

 
Resolution: The solid state overload relays do not need thermal units.


Keywords: thermal units, solid state overload relay, SSOLR
 
 
Was this helpful?
What can we do to improve the information ?