Technical FAQs

Ask a Question

What is the mounting plate part number for an ATV71HU15N4?

Issue:
What is the mounting plate part number for an ATV71HU15N4?
Product Line:
ATV71/ ATV61
Environment:
 ATV71HU15N4 ATV71HU15M3 ATV71HU22M3 ATV61H075N4 ATV61HU15N4 ATV61HU22N4 ATV61HU15M3
Cause:
N/A
Resolution:
The part number for the mounting plate for an ATV71HU15N4 is VW3A9302
Kit includes: Mechanical adaptors required for mounting an Altivar™ 61/71 drive in the
place of an Altivar 58 or Altivar 58F drive using the same holes.
Was this helpful?
What can we do to improve the information ?