Technical FAQs

Ask a Question

Does the HOM3060M200PC comes with a ground bar if not what ground bar is needed?

Issue:
Selection

Product Line:
Homeline Load Center

Environment:
Applies to HOM3060M200PC

Cause:
Selection

Resolution:
The HOM3060M200PC will accept any of the ground bars from PK9GTA through PK27GTAL. The PK23GTA is recommended based on the number of circuits available in the load center.
Was this helpful?
What can we do to improve the information ?