Technical FAQs

Ask a Question

What Generator Interlock Kit can be used with the HOM2448L125PGC Series S04 / S4 Load Center?

Issue:
Selection

Product Line:
Homeline Load Center

Environment:
Applies to HOM2448L125PGC series S04 loadcenter.

Cause:
Selection

Resolution:
The HOM2448L125PGC is a Main Lugs Only panel. In order to use a Generator Interlock Kit with this panel, it would first have to be converted to a Main Breaker panel by removing the main lugs and installing a QOM1-VH Main Breaker Kit, 125A maximum. The Generator Interlock Kit HOMCRBGK1 could then be used to interlock between a backfed generator breaker, 125A maximum, and the QOM1-VH main breaker.
Was this helpful?
What can we do to improve the information ?