Technical FAQs

Ask a Question

What is the bus rating for SC3040M200F Series M01 or M02?

Issue:
Application

Product Line:
CSED

Environment:
Application
 
Cause:
Application 

Resolution:
The bus rating is equal to the maximum mains marked on the wiring diagram: 225 A.
Was this helpful?
What can we do to improve the information ?