Technical FAQs

Ask a Question

What terminals are used for the 4-20ma external signal on the 8839 E-Flex enclosed drives?

Issue:
What terminals are used for the 4-20ma external signal on the 8839 E-Flex enclosed drives?

Product Line:
8839 E-Flex enclosed drives

Environment:
All

Cause:
Needs to know where to wire up his 4-20ma signal for auto speed control. 

Resolution:
wire your 2-20mA or 4-20mA auto signal to JS2 +and JS3 -
Was this helpful?
What can we do to improve the information ?