Technical FAQs

Ask a Question

What is the standard wire range for the LJL tenant breaker used in the Series M03, EZM 400amp branch devices?

Issue:
Tenant breaker wire range

Product Line:
EZM Metering 

Environment:
standard Wire sizes 

Cause:
Metering application

Resolution:
The standard wire range for the LJL36400U31X tenant breaker, used in the Series M03, EZM 400A branch devices, will accept as standard (2) 2/0 - 500kcmil AL/CU wires.

NOTE: There is an optional single barrel lug for this tenant breaker, kit catalog number AL400L61K3 (kit includes 3 lugs) and this lug will accept (1) #2 AWG - 600kcmil CU wire OR (1) #2 AWG - 500kmil AL. wire.  

 
Was this helpful?
What can we do to improve the information ?