Technical FAQs

Ask a Question

Can a 500-690V ATV61 series drive be used with a permanent magnet, synchronous motor?

Issue:
Can a 500-690V ATV61 series drive be used with a permanent magnet, synchronous motor?

Product Line:
Altivar 61 series

Environment:
ATV61xxxxY models, all serial numbers

Cause:
Customer has a 600V permanent magnet synchronous motor for use in a ventilation application and is looking for a suitable drive.

Resoultion:
No, The 500-690V ATV 61 drives (Y version) can not operate synchronous, permanent magnet motors.  The 208-230 and 380-480V seris drives (M3, N4) can but only if the motor has sinusodial EMF.
Was this helpful?
What can we do to improve the information ?