Technical FAQs

Ask a Question

Is a white cover available for the HOM2448M100PC load center?

Issue:
Product availability

Product Line:
HOMELINE load center

Environment:
Non standard cover

Cause:
Customer preference

Resolution:
Yes, it is. The HOM2448M100PC will come with the standard gray (ANSI-49) cover provided. To purchase a separate white cover, order HOMC24UCW.
 
Was this helpful?
What can we do to improve the information ?