Technical FAQs

Ask a Question

Is there an ethernet communication option for the ATV32 drive?

Issue:
Is there an ethernet communication option for the ATV32 drive?

Product Line:
ATV32

Environment:
All models
 
Cause:
Product Selection & Services

Resolution:
Yes ,   Part number  VW3A3616    Ethernet IP—Modbus™ TCP/IP daisy chain option card, two RJ45 ports 10/100 Mbps, half duplex and full duplex, embedded web server,
 
 Network Communication Option Cards
 The Altivar 32 can accept one of the following network communication option cards. The card slides into the Altivar 32
 without taking up addition panel space, CANopen from the embedded port is disabled when an option card is installed.
 
Was this helpful?
What can we do to improve the information ?