Technical FAQs

Ask a Question

How can you identify a 9070FSC2, finger safe terminal cover?

Issue:
How can you identify a 9070FSC2, finger safe terminal cover?

Product Line:
9070T, 9070TF

Environment:
Industrial Control Transformes

Cause:
Identifing covrs for the 9070T and 9070TF Control Transformers

Resolution:
The covers themselves do have the part number embossed on the plastic. You have to hold them up to the light
to see the number. Look along the edge that faces the top of the transformer, not the vertical
section that points downward.
Was this helpful?
What can we do to improve the information ?