Technical FAQs

Ask a Question

Will the old style(Non-PoN) Homeline and QO, CAFI and DF breakers fit into the new style Plug-On Neutral Homeline and QO load centers?

Issue:
Application

Product Line:
QO and Homeline

Environment:
Homeline and QO load centers sold and supported in the US

Cause:
Clarification

Resolution:
Yes. The new style Plug-On Neutral QO and Homeline load centers will accept either styles of CAFI and DF breakers, Plug-On Neutral or traditional pigtail type. The white pigtail wire would attach to the load center neutral bar.

 

Was this helpful?
What can we do to improve the information ?