Technical FAQs

Ask a Question

What is the UL wire specification for the NSYTRP24DPE terminal block?

Issue:
What is the UL wire specification for the NSYTRP24DPE terminal block?
Product Line:
Linergy TR Screw terminal blocks.
Environment:
Linergy TR NSYTRP24DPE
Cause:
To clarify the wire selection for the customer’s application.
Resolution:
600V, 20 A, 26-12 AWG, which is found on page 64 in the LINERGY CATALOG 9080CT1301
 
Was this helpful?
What can we do to improve the information ?