Technical FAQs

Ask a Question

What are the UL wire specification for the NSYTRP22PE terminal block ?

Issue:
What are the UL wire specification for the NSYTRP22PE terminal block?
Product Line:
Linergy TR Screw terminal blocks.
Environment:
Linergy TR NSYTRP22PE
Cause:
To clarify the UL specifications for a particular application
Resolution:
24-12AWG wire, found on page 62 in the LINERGY CATALOG 9080CT1301
 
Was this helpful?
What can we do to improve the information ?