Technical FAQs

Ask a Question

What is the UL wire specification for the NSYTRP44 terminal block?

Issue:
What is the UL wire specification for the NSYTRP44 terminal block?
Product Line:
Linergy TR Screw terminal blocks.
Environment:
Linergy TR NSYTRP44, NSYTRP44BL,
Cause:
To clarify the wire selection for the customer’s application.
Resolution:
600V, 30A, 24-10AWG, which is found on page 61 in the LINERGY CATALOG 9080CT1301
 
Was this helpful?
What can we do to improve the information ?