Technical FAQs

Ask a Question

Why does the fan on my drive run continously when it is cold?

Issue:
Fan continues to run

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
The fan should not run continously.  The fan should come on when the drive thermal state reaches 70% and stop when it drops below 60%.

Resolution:
The drive can operate with the heatsink fan running continously.  If this is undesirable the drive can be repaired or replaced.
Was this helpful?
What can we do to improve the information ?