Technical FAQs

Ask a Question

What is the replacement coils for AC Magnet coils for 9050 Type B Timers?

Issue:
What is the replacement coils for AC Magnet coils for 9050 Type B Timers?

Product Line:
Replacement 9050 Timer

Environment:
Products sold in North America

Cause:
Need to replace the coil in a 9050 Timer

Resolution:
 


 
Coil Voltage (V) 60 Hz 50 Hz
24 31017-400-33
120 31017-400-54
208 31017-400-61
220 31017-400-63
240 31017-400-63
277 31017-400-65
440 31017-400-72
480 31017-400-72
550 31017-400-75
600 31017-400-75  
 
  Coil VA
  In Rush Sealed
60 Hz 165 27
50 Hz 155 27
Was this helpful?
What can we do to improve the information ?