Technical FAQs

Ask a Question

What is the difference between the HFVS1 and the HFVS2?

Issue:
What is the difference between the HFVS1 and the HFVS2?

Product Line:
Busway Hangars

Environment:
I-line II Busway hangars

Cause:
Installation, product features

Resolution:
The hangars are the same. There is no physical difference. The difference is the quantity of hangars included in the kits.
The HFVS1 kit has 1 hangar. The HFVS2 kit has 2 hangars.
 

Was this helpful?
What can we do to improve the information ?