Technical FAQs

Ask a Question

Which ATV61 / ATV71 drives are frame size 8?

Issue:
Which ATV61 / ATV71 drives are frame size 8?

Product Line:
ATV61 ATV71

Environment:
All 460V/480V

Cause:
Possible alternatives

Resolution:
ATV71HD45N4, ATV71HD55N4, ATV71HD75N4
ATV61HD45N4, ATV61HD55N4, ATV61HD75N4
Was this helpful?
What can we do to improve the information ?