Technical FAQs

Ask a Question

Are the new Plug-ON Neutral Homeline Load Centers Convertible as the old Homeline Catalog numbers were?

Issue:
Current design features

Product Line:
Homeline Load centers

Environment:
Convertible Mains

Cause:
Main Breaker and Main Lugs

Resolution:
ALL the old Homeline catalog numbers that WERE convertible(Main lug to Main breaker OR Main Breaker to Main Lug) would carry over to their new Plug-On Neutral Catalog number counterparts and would also be converitble. 
Was this helpful?
What can we do to improve the information ?