Technical FAQs

Ask a Question

What are the dimensions of the QOC342MQS load center cover?

Issue:
Dimensions

Product Line:
QO Load Center

Environment:
Dimensions

Cause:
Dimensions

Resolution:
A surface cover will be the same height and width of the load center enclosure that it mounts to. The QOC342MQS is 14.25" W x 39.37" H.
Was this helpful?
What can we do to improve the information ?