Technical FAQs

Ask a Question

What are the dimensions of the QOC342MQF load center cover?

Issue:
Dimensions

Product Line:
QO Load Center

Environment:
Dimensions

Cause:
Dimensions

Resolution:
A flush cover will extend past the sides of the load center enclosure by .60" on all sides. The QOC342MQF is 15.45" W x 40.57" H.
Was this helpful?
What can we do to improve the information ?