Technical FAQs

Ask a Question

Can you order the top cover plate that goes over where the DC choke is mounted on the high HP ATV61 and ATV71 drives?

Issue:
Can you order the top cover plate that goes over where the DC choke is mounted on the high HP ATV61 and ATV71 drives?

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
HP

Cause:
The customer has removed the DC choke and needs the top cover to mount on the drop of the drive.

Resolution:
We do not sell the top plate to cover up the area where the DC choke was removed on the high HP ATV61 71 drives.
 

Was this helpful?
What can we do to improve the information ?