Technical FAQs

Ask a Question

What is the Terminal Lug Data and alternate lugs for the EZM11200GCBU Main Device?

Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Environment:
EZM Main Breaker lugs

Cause:
Standard terminations

Resolution:
The EZM11200GCBU will accept as standard (4) 3/0 to 500kcmil AL/Cu wires per phase and neutral and (1) # 6 - 300kcmil Al/Cu wire per ground lug.
SEE THE CAD DRAWING #PWFDS-SYRS-0034 FOR OPTIONAL LUGS

NOTE: Any of the Alternate Lugs shown on the above CAD drawing will REQUIRE the use of the Lug Landing Kit catalog number EZM1200ULL(purchase separately)


 

Was this helpful?
What can we do to improve the information ?