Technical FAQs

Ask a Question

Replacement handle for legacy PA, PH, PC, PX and PE frame breakers

Issue:
Is there a replacement for just the handle on the older PA, PH, PC, PX and PE frame legacy circuit breakers?

Product Line: 
P-frame circuit breakers

Environment:
Maintenance/repair 

Cause:
The P frame handle required more torque to operate and material fatigue over time can cause the handle to break. 

Resolution:
Yes, the part number is HRPA
Was this helpful?
What can we do to improve the information ?