Technical FAQs

Ask a Question

What is the length of the hookstick used to operate a busway plug in unit?

Issue:
Hookstick used to operate a busway plug in unit

Product Line:
Busway 

Environment:
I-Line

Cause:
Dimension hookstick are required.

Resolution:
The length of 515608 (8ft-previously 51568) and 515614 (14 ft)
 
Was this helpful?
What can we do to improve the information ?