Technical FAQs

Ask a Question

What positions does the backfed main breaker install into in a HOM612L100S loadcenter?

Issue:
Installation

Product Line:
Homeline

Environment:
Back fed main

Cause:
Installation requirement

Resolution:
The backfed main breaker must be installed in positions 1 and 2. A retaining kit, HOM1RK, must be used to secure the backfed main to the interior. This information is validated on the wiring diagram of the device.


CTA-ID : 2028496
Was this helpful?
What can we do to improve the information ?