Technical FAQs

Ask a Question

Does LCSADVANCEDUP or LCSBASICUP have a front panel cable?

Issue:
Customer purchased LCS Software but it does not have a cable to connect to Powerlink controller.  

Product Line:
Powerlink Lighting Control System
NF Panelboards

Environment:
Commercial Lighting Control

Cause:
The standard versions of LCSADVANCED and LCSBASIC include a Powerlink Front Panel Cable NFFPCG3.  There are "Upgrade" versions of LCS are intended for customers who previously owned the predecessor software, PCS.  These Upgrade versions are LCSADVANCEDUP and LCSBASICUP.   PCS software used the same Front Panel Cable; thus, the Upgrade versions do not include the cable.  

Resolution:
The Front Panel Cable, NFFPCG3, can be ordered separately.
If the Powerlink Controller is NF2000G3, NF3000G3, or NF3000G3C, then one could connect to the internal Ethernet port without a special cable.   
 
Was this helpful?
What can we do to improve the information ?