Technical FAQs

Ask a Question

Can you use any of the ATS soft starters to feed an transformer to get higher voltage out?

Issue:
They want to use a soft starter to reduce the input currents coming into a transformer.

Product line:
Alitstart soft starters ATS01 ATS23 ATS46 ATS48 ATS22

Environment:
All models

Cause:
Inrush current is too high in the installation

Resolution:
We do not recommend the use of the Altistart soft starters feeding into a transformer.
 

Was this helpful?
What can we do to improve the information ?