Technical FAQs

Ask a Question

Do Speed D switchboards ending in WS or WR have provisions for adding an interior, 400A branch, subfeed breakers or the QO plug on kit?

Issue:
Do Speed D switchboards ending in WS or WR have provisions for adding an interior, 400A branch,  subfeed breakers or the QO plug on kit?

Product Line:
Switchboards

Environment:
Speed D switchboards

Cause:
Installation, Product Features

Resolution:
No. Speed D switchboards ending in WS or WR only have provisions for the main. There is no bussing
available to add an interior, subfeed breaker, QO plug in kit, or an additional 400A breaker.
 

Was this helpful?
What can we do to improve the information ?