Technical FAQs

Ask a Question

What is the part number for the ATV61 modbus card that gives you the 9 pin sub D connector similar to what was used on the ATV58 TRX series with modbus option?

Issue:
What is the part number for the ATV61/71 modbus card that gives you the 9 pin sub D connector similar to what was used on the ATV58 TRX series with modbus option?

Product Line:
Altivar ATV61 and ATV71

Environment:
All with VW3A3303 modbus option card

Cause:
They are converting over drives from the old ATV58 to the new ATV61 with modbus so they need a modbus card with the same 9 pin sub D connector that was on the ATV58 modbus card.

Resolution:
If you add the VW3A3303 modbus option card this will give you the 9 pin sub D connector that was used on the old ATV58 modbus cards.
Reference VW3A3303 manual that is attached.

Was this helpful?
What can we do to improve the information ?